LPC Parametric Table?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Parametric Table?

685件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by clement738 on Thu Sep 23 09:38:13 MST 2010
Hi all,
This is my first post. Where can I get the LPC parametric table which list all nxp lpc in a table format, so that it is easy to select the lpc for our application.

Also, is there any lpc with built-in SRAM more than 64K? I'm looking for a lpc with 256K SRAM.

Thanks.


Clement
0 件の賞賛
返信
1 返信

675件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Sep 23 09:58:25 MST 2010
[LEFT]Perhaps:[/LEFT]

[LEFT]http://ics.nxp.com/products/mcus/cortex-m3/[/LEFT]

[LEFT]Some of the LPC17xx have more than 64k, see link above :). [/LEFT]
0 件の賞賛
返信