Weirdness in UARTs during debug session

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Weirdness in UARTs during debug session

1,067 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JGold on Thu Sep 23 06:49:12 MST 2010
When I am running the debugger, and look at the peripheral window for UART2, I get incorrect feedback.  See the attached clip.  The register UDLM at address 0x40098004 has bits listed under it for the modem signals for UART1 U1MSR register.  Also, UART2 UDLL does not report correctly for the baudrate I am running.  Lastly, UART3 is being used, but is being shown as disabled.[ATTACH]192[/ATTACH]
0 Kudos
Reply
3 Replies

1,061 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 23 08:23:28 MST 2010
This has now been fixed and will be in the next release of LPCXpresso.

Thanks for reporting it.
0 Kudos
Reply

1,061 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JGold on Thu Sep 23 07:11:07 MST 2010
Lpc1765
0 Kudos
Reply

1,061 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 23 07:10:00 MST 2010
Hi,

Can you tell us which part you are using?
0 Kudos
Reply