LPC-Link2 enclosure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link2 enclosure

7,897件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gbrus on Sat Aug 09 02:29:55 MST 2014
As the LPC-link2 debugger doesn't have an enclosure and a short cable, I always had to be careful not to have the LPC-link2 and the board I'm working getting to close to each other and damage one (or both) of them. So I made a enclosure for the LPC-Link2 and had it printed with a 3D-printer.
I like to share the STL models with you, so if any of you have access to a 3D-printer you can easily make an enclosure for you LPC-Link2.

The LPC-Link2 can be mounted with 2 screws and there are slots for all the cables to get out of the enclosure. Through the hole in the cover the LED is still visible, with a light pipe even better (it's diameter is to fit the Bivar PLP2 light pipes).

I hope it will be useful to some of you.

Original Attachment has been moved to: LPC-Link2%20enclosure.rar

3 返答(返信)

7,702件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gbrus on Tue Aug 12 08:25:43 MST 2014
As promised, pictures of the LPC-Link2 enclosure printed (with a Stratasys 3D-printer, ABS material).

[img]http://www.lpcware.com/system/files/LPC-Link2-1.jpg[/img]

[img]http://www.lpcware.com/system/files/LPC-Link2-2.jpg[/img]
0 件の賞賛
返信

7,702件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Gbrus on Sat Aug 09 11:33:35 MST 2014
I will post a picture of it a.s.a.p.
0 件の賞賛
返信

7,701件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sat Aug 09 05:08:19 MST 2014
Very nice idea  :)

Perhaps you can show us a picture?

Meanwhile it looks promising in FreeCAD...

[img]http://www.lpcware.com/system/files/C1.jpg[/img]

[img]http://www.lpcware.com/system/files/C2.jpg[/img]
0 件の賞賛
返信