QEI register read or write hard fault handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QEI register read or write hard fault handler

868件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cbureau on Sat Nov 17 11:05:40 MST 2012
Hello, i try to connect a quadrature encoder on Lpcxpresso lpc1769 board, but when i execute this simple code :
LPC_QEI->CON |=  1;
I optain an hard fault handler:(.
when i debug my example.
can i have an help please ?
Thanks

Now it's good , just a little error in my (#define declaration) . sorry.
0 件の賞賛
返信
1 返信

844件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Nov 17 11:25:35 MST 2012
PCONP bit 18 PCQEI Quadrature Encoder Interface power/clock control bit :confused:
0 件の賞賛
返信