LPC-Link & Windows 10 driver Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link & Windows 10 driver Problem

19,238件の閲覧回数
gmin
Contributor I

Hi,
I've install LPCXpresso v8.2.2 [Build 650] [2016-09-09]  in a Windows 10 - 64 bits PC.
When I've connected LPC-Link1 to the USB, LPCExpresso does not recognize it.
I've deleted the driver Driver and then connect the LPC-Link and it had been detected as a DFU device.

Then I've reinstalled the driver from c:\nxp\LPCXpresso_8.2.2_650\Drivers\LPC-Link\ (See Images) but the LPC link driver seems to be not the correct for Win10. After that, LPC Expresso still not recognize it.
Is there another driver version for Windows 10-64 bits ?
I've already probed with 2 different LPC-Link devices and 2 different Mini USB cables.

Urgent response will be appreciated.

Regards,
Gus

ラベル(3)
0 件の賞賛
返信
5 返答(返信)

17,040件の閲覧回数
bobarry
Contributor I

I too cannot get my LPCXpresso11u68 recognized on windows 10.  Drivers and software installed OK, but nothing is recognized when its connected to the link connector with jumper 1 off, jumper 2&3, and dfu off.

Got it at a ham radio swap fest. It looks handy for use with MBED which I am familiar with.

No connection so the MBED update wouldn't take,

Any help appreciated.

Bo W4GHV

0 件の賞賛
返信

17,040件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

There is no updated LPC-Link driver. We have not seen any issues ourselves using LPC-Link on Windows 10. What is the exact version of Windows that you are using?

In the first place, please run through the FAQ: https://community.nxp.com/thread/388960 

Regards,

LPCXpresso Support

0 件の賞賛
返信

17,039件の閲覧回数
gmin
Contributor I

Hi.

    I'm using Windows 10 - Home Edition

I'm without clues....

regards,

Gustavo

0 件の賞賛
返信

17,039件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Did you try going through the FAQ previously referenced?

Regards,

LPCXpresso Support

0 件の賞賛
返信

17,039件の閲覧回数
gmin
Contributor I

Yes, I did.

Still Not working on LPCXpresso 8....

0 件の賞賛
返信