Debugging with source codes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging with source codes

538 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shintamainjp on Tue Feb 22 03:48:18 MST 2011
I was fixed a problem in http://knowledgebase.nxp.trimm.net/showthread.php?t=1589.

So I checked the feature of the board.
And I found a problem in it.

I have two LPCXpresso LPC1768 boards.

I can't see any source codes with a board in debugging.
But I can see source codes with the other board with the same project.

How do I reset the board to initial statement.
:confused:

Program is not running. (Secondary boot loader broken?)

Sorry, I created two problems in a day. :(

Best regards,
Shin.

P.S. I executed bootLPCXpresso.cmd to the board. What's this?
0 Kudos
Reply
0 Replies