Debug/Download to RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug/Download to RAM

1,176件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Sun Apr 20 10:29:13 MST 2014
Hello,
after digging out my LPCXPresso LPC11C24 I updated from LPCXpresso 6 (maybe 5)  to 7. Because I make a lot of of tiny modifications I usually downloaded my 'applications' to RAM to save the flash live time. Therefore I just set SYSMEMREMAP to 0x1 in SystemInit() and modified in the MCU settings MFlash32 to 0x10000000 (size 0x1C00) and RamLoc8 to 0x10001C00). In the past that worked fine. But now I get

15: Target error from Register access
Cannot complete transaction, even after slowing speed.

and in console
...
v LPCXpresso Free License - Download limit is 256K
Executing in user flash.
SYSPLLSTAT read: Em(11). Cannot complete transaction, even after slowing speed.
Stopped: Locked-up, Sleeping, In-reset (Was Reset)  [Reset from  PowerOn, External, Watchdog, BrownOut, SysRes]: VectorCatch:Reset (PC unknown: cannot read registers) (VectorCatch,Breakpoint,Watchpoint,EDBGRQ)
Target error from Register access: Em(11). Cannot complete transaction, even after slowing speed.

when I start debugging. Did I forget something important in the last year or has something changed?
0 件の賞賛
返信
4 返答(返信)

1,129件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Tue Apr 29 01:08:28 MST 2014

Quote: R2D2

Quote: 1234567890
...to save the flash live time.



:quest:

You are kidding? How long does your flash live?



Not really. Datasheet says a minimum of 10.000 write cycles. With about 150-200 writes a day it can become an issue.
But you're right: That only happens when I do it every day. And that is not the fact and the device should withstand at least 2 years.


Quote: 1234567890
Did I forget something important in the last year or has something changed?



Did you try to boot into ISP already?
No, but I can't remember doing that before.
0 件の賞賛
返信

1,129件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by 1234567890 on Tue Apr 29 07:40:26 MST 2014
Interesting result; thank you.
So I probably won't flash my device to death.
0 件の賞賛
返信

1,129件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Apr 29 02:19:29 MST 2014
Tests are showing that Flash endurance is probably higher...

http://www.lpcware.com/content/forum/real-iap-wear-out-data

So you could flash it 20 years 200 times/day.  Until 2034  :)
0 件の賞賛
返信

1,129件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sun Apr 20 10:49:16 MST 2014

Quote: 1234567890
...to save the flash live time.



:quest:

You are kidding? How long does your flash live?



Quote: 1234567890
Did I forget something important in the last year or has something changed?



Did you try to boot into ISP already?
0 件の賞賛
返信