Activating LPCXpresso Pro Edition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Activating LPCXpresso Pro Edition

4,508件の閲覧回数
lpcware-support
Senior Contributor I

To enable the features of LPCXpresso (Pro Edition), a activation code must be purchased from the NXP LPCXpresso webstore.

The first time this Activation code is used, the following steps are required:

Within the LPCXpresso IDE product select:

  • Help -> Activate -> Activate Pro Edition
  • and enter the supplied activation code.

145132_145132.pngpastedImage_0.png

  • enter a valid email address
  • enter a password to be associated with this Activation code

145136_145136.pngpastedImage_1.png

The email address supplied for the first activation is used by Softworkz, our license systems supplier, to send a Welcome Email with the Subject 'myLicense Portal Information'. This Welcome mail is important and should be kept by the user or administrator.

The supplied password is now associated with this activation code and should be kept safe as it is required to deactivate (remove) or to reactivate LPCXpresso IDE (Pro Edition).

Multi Seat Activation Codes

Multi Seat activation codes allow LPCXpresso IDE (Pro Edition) to be activated on multiple machines, until all seats have been used. So a 5 seat Activation code allows LPCXpresso IDE (Pro Edition) to be activated onto 5 unique computers. After the initial activation (as described above), all subsequent installations simply require the password that has been associated with the Activation code.

Within LPCXpresso IDE product select:

  • Help -> Activate -> Activate Pro Edition
  • enter the Multi Seat Activation code
  • enter the password that has been associated with that Activation code.

145137_145137.pngpastedImage_2.png

Related FAQs


ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)