porting Emwin to LPC1549 / LPC1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

porting Emwin to LPC1549 / LPC1768

2,049件の閲覧回数
allwyn
Contributor I

Hi,

we are working on LPC1549 with a TFT LCD display. i understand that NXP provides pre-compiled  lib of emWin.Is there  any beginner guide to port the same on cortex M3 .Display has ili9481 display controller

We use IDE-MCUxpresso

Please share Any application  note /successful project links/information .

ラベル(3)
0 件の賞賛
返信
1 返信

1,783件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ALLWYYN ANTONY,

   Yes, we have the application note and the emwin sample code for LPC1769, please refer to these link:

  1. https://www.nxp.com/docs/en/application-note/AN11244.pdf 

  

   2. Code issue solutions in emWin_mcb1700_bsp 

   The sample code is using the LPXpresso IDE, but don't worry, the MCXpress IDE totally compatible with the LCXpresso IDE, you can open the LPCXpesso IDE project with MCUXpresso IDE directly.

Please try it on your side.

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信