porting Emwin to LPC1549 / LPC1768

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

porting Emwin to LPC1549 / LPC1768

2,047 Views
allwyn
Contributor I

Hi,

we are working on LPC1549 with a TFT LCD display. i understand that NXP provides pre-compiled  lib of emWin.Is there  any beginner guide to port the same on cortex M3 .Display has ili9481 display controller

We use IDE-MCUxpresso

Please share Any application  note /successful project links/information .

Labels (3)
0 Kudos
Reply
1 Reply

1,781 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ALLWYYN ANTONY,

   Yes, we have the application note and the emwin sample code for LPC1769, please refer to these link:

  1. https://www.nxp.com/docs/en/application-note/AN11244.pdf 

  

   2. Code issue solutions in emWin_mcb1700_bsp 

   The sample code is using the LPXpresso IDE, but don't worry, the MCXpress IDE totally compatible with the LCXpresso IDE, you can open the LPCXpesso IDE project with MCUXpresso IDE directly.

Please try it on your side.

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply