lpc812 mbed keeps disconnecting, showing as a usb drive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

lpc812 mbed keeps disconnecting, showing as a usb drive

跳至解决方案
1,411 次查看
svensavic
Contributor III

I think something is wrong with my board. I just received it, so I dont know what is suppose to be the normal operation, but this for sure seems like a malfunctioning board.

My board keeps connecting/disconnecting from my laptop. Shows as a portable device in device manager and it brings the "usb drive" with mbed.htm file and fail.txt which contains string "TIMEOUT". It keeps flashing D4 USB Disk LED and D3 and D5 are on. I cannot connect to it through LPCXpresso 8.2.

If I put the power on while holding the reset button, then I get usb drive with firmware.bin file in it. Still not connecting to LPCXpresso.

Any tips ? Or should I return the board and ask for new one ?

Thanks

标记 (2)
0 项奖励
回复
1 解答
1,220 次查看
svensavic
Contributor III

Ok, it seems that my board have had bad firmware. Installing the new 0203 fw fixed the disconnect problem. And then installing the virtual serial driver fixed the CMSIS-DAP connection to LPCXpresso.

It is working ok now. I am just puzzled how did I got new board with malfunctioning firmware...

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,221 次查看
svensavic
Contributor III

Ok, it seems that my board have had bad firmware. Installing the new 0203 fw fixed the disconnect problem. And then installing the virtual serial driver fixed the CMSIS-DAP connection to LPCXpresso.

It is working ok now. I am just puzzled how did I got new board with malfunctioning firmware...

0 项奖励
回复