is there any Emulated EEPROM driver for LPC802

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

is there any Emulated EEPROM driver for LPC802

ソリューションへジャンプ
3,174件の閲覧回数
naveenkumar_b
Contributor II

Hi,

I am using LPC802 16kb flash controller. I would like to retain and change few parameters by using configurator. I don't want to use external EEPROM. Is there any is there any Emulated EEPROM driver for LPC802 controller.

Regards,

Naveen

ラベル(1)
0 件の賞賛
返信
1 解決策
3,006件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Naveen Kumar,

    We have an application named as AN12125 Using LPC802 as I2C-bus EEPROM, this application will simulate the LPC802 chip as the eeprom, it also contains the code, it use the flash as the eeprom storage, just what you want to have, please download this application note.

Wish it helps you!
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
3,007件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Naveen Kumar,

    We have an application named as AN12125 Using LPC802 as I2C-bus EEPROM, this application will simulate the LPC802 chip as the eeprom, it also contains the code, it use the flash as the eeprom storage, just what you want to have, please download this application note.

Wish it helps you!
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,739件の閲覧回数
biju_nair
Contributor III

Hi,

This link seems broken. Any new link available ?

Regards, Biju

0 件の賞賛
返信
3,006件の閲覧回数
naveenkumar_b
Contributor II

Thanks

0 件の賞賛
返信