guide for flash programming via usb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

guide for flash programming via usb

3,290 次查看
larry781111
Contributor I

The EVB is OM40005, for now I use GUI Flash Tool to flash my binary code into LPC51U68.

But I would like to customize my board and flash my binary code via USB_DP and USB_DM, is it available?

Which programming software should be used to flash the code?

标记 (2)
0 项奖励
回复
1 回复

2,952 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi YuChia Chien,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
It's available to upgrade the application code via the USB ISP.
When plugging in the USB port of the PC, the MCU will be emulated as a driver if it already enters the USB ISP mode, you can drop the BIN to the driver to upgrade the application code.

pastedImage_1.png
Hope it helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复