guide for flash programming via usb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

guide for flash programming via usb

3,382件の閲覧回数
larry781111
Contributor I

The EVB is OM40005, for now I use GUI Flash Tool to flash my binary code into LPC51U68.

But I would like to customize my board and flash my binary code via USB_DP and USB_DM, is it available?

Which programming software should be used to flash the code?

タグ(2)
0 件の賞賛
返信
1 返信

3,044件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi YuChia Chien,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
It's available to upgrade the application code via the USB ISP.
When plugging in the USB port of the PC, the MCU will be emulated as a driver if it already enters the USB ISP mode, you can drop the BIN to the driver to upgrade the application code.

pastedImage_1.png
Hope it helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信