eRPC support for LPC546xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eRPC support for LPC546xx

ソリューションへジャンプ
5,291件の閲覧回数
gbarcan
Contributor II

Hi,

Is eRPC supported on the LPC546xx ? Would anybody be able to offer any advice or guidance on using eRPC LPC546xx ?

Any help would be appreciated, 

Thank you,

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,104件の閲覧回数
dusancervenka-b
NXP Employee
NXP Employee

Hi [email protected]‌,

officially there is no example ported for this board. But eRPC doesn't has dependency for board. He has dependency for used OS and transport layer. 

For more information you can look on this documentation: https://community.nxp.com/docs/DOC-334083

And here for step-by-step guide how to create erpc application: https://github.com/EmbeddedRPC/erpc/wiki/Getting-Started

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,104件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

In addition, you can check the following thread 

https://community.nxp.com/thread/477242

I hope this helps, 

Have a nice day!

Soledad

0 件の賞賛
返信
5,104件の閲覧回数
gbarcan
Contributor II

eRPC (embedded remote procedure call) and ECRP (Enhanced Code Read Protection)

0 件の賞賛
返信
5,105件の閲覧回数
dusancervenka-b
NXP Employee
NXP Employee

Hi [email protected]‌,

officially there is no example ported for this board. But eRPC doesn't has dependency for board. He has dependency for used OS and transport layer. 

For more information you can look on this documentation: https://community.nxp.com/docs/DOC-334083

And here for step-by-step guide how to create erpc application: https://github.com/EmbeddedRPC/erpc/wiki/Getting-Started

0 件の賞賛
返信
5,104件の閲覧回数
gbarcan
Contributor II

Thank you Dusan, I think we should be able to get it running on the LPC546xx using the uart transport and through the CMSIS UART Driver. We started working on it and we should have hardware available soon to test things.

0 件の賞賛
返信