can LPC54S018M with External SPI boot run in XIP mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can LPC54S018M with External SPI boot run in XIP mode?

1,876 Views
belmontbob59
Contributor IV

Which options are available to run in XIP besides internal SPIFI flash?  Can we run code in external SPI flash connected to the MCU via FC9 in XIP mode? 

from 54S018M's manual (UM11155):

pastedImage_1.png

Thank you

Labels (1)
0 Kudos
Reply
3 Replies

1,832 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi bob

Yes, you can run code in external SPI flash connected to the MCU via FC9 in XIP mode.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,832 Views
belmontbob59
Contributor IV

thank you for the prompt reply

0 Kudos
Reply

1,832 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 Kudos
Reply