can LPC54S018M with External SPI boot run in XIP mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can LPC54S018M with External SPI boot run in XIP mode?

1,890件の閲覧回数
belmontbob59
Contributor IV

Which options are available to run in XIP besides internal SPIFI flash?  Can we run code in external SPI flash connected to the MCU via FC9 in XIP mode? 

from 54S018M's manual (UM11155):

pastedImage_1.png

Thank you

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,846件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi bob

Yes, you can run code in external SPI flash connected to the MCU via FC9 in XIP mode.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,846件の閲覧回数
belmontbob59
Contributor IV

thank you for the prompt reply

0 件の賞賛
返信

1,846件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信