What the highest transfer rate can be using USB1 as a vcom?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What the highest transfer rate can be using USB1 as a vcom?

3,031 Views
yanlong_gao
Contributor I

I was testing with the dev_cdc_vcom_bm example from MCUXpresso SDK, and an LPCXpresso54628 eval board.

I can configure the USB device worked in high-speed mode, and it's about 4MB/s when sending data to PC.

I want to know what the highest transfer rate can be,  could it reach to 40MB/s as mentioned here https://community.nxp.com/message/760578

0 Kudos
Reply
7 Replies

2,911 Views
yanlong_gao
Contributor I

if I use the USB1 as a virtual com port, can that speed also be reached? and how?

0 Kudos
Reply

2,911 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Since you use USB1 as virtual com, the speed limitation is not on USB1 but your virtual com device.

What speed your virtual com device can reach?

0 Kudos
Reply

2,911 Views
yanlong_gao
Contributor I

What do you mean by virtual com device?

I am running the dev_cdc_vcom_bm example from SDK, the USB1 will be recognized as a virtual com port from the PC, LPC board send data through USB1 to PC, and PC read data through the virtual com port, the speed can reach to about 4MB/s.

My question is what's the highest speed can reach? some people said that could reach to 40MB/s, and that sounds reasonable since the high-speed USB can reach to a 480Mb/s about 60MB/s.

0 Kudos
Reply

2,911 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

OK, understand.

In your case, the USB1 as virtual COM, the high-speed USB can reach to 480Mb/s.

0 Kudos
Reply

2,911 Views
yanlong_gao
Contributor I

OK, thanks.

Maybe I should change the title of this question to HOW to reach to 480Mb/s.

0 Kudos
Reply

2,911 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 Kudos
Reply

2,911 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi will hunt 

According to LPC546xx datasheet, USB1 speed can reach 480Mbit/s.

pastedImage_1.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply