What's wrong with M4 reset (M4_RST) on LPC43x0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What's wrong with M4 reset (M4_RST) on LPC43x0?

2,246 Views
danstahlke
Contributor II

The errata sheet says M4_RST is not functional on LPC43x0.  But I tried it on LPC4370 revisions C and D and it seems to work.  Is the errata wrong, or is this function broken in some subtle way?

If M4_RST really can't be used, is there a way to simulate reset (for the purpose of a bootloader) without resetting GPIO configuration?  I don't like the pulses that come out of the I/O pins when doing a hard reset.

Labels (1)
0 Kudos
Reply
3 Replies

2,119 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Dan Stahlke,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
1) Is there a way to simulate reset (for the purpose of a bootloader) without resetting GPIO configuration?  
-- Unfortunately, there is no workaround.
Have a great day,
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 Kudos
Reply

2,119 Views
danstahlke
Contributor II

Do you happen to know why M4_RST is listed as non-functional in the errata?  I've been using it and it seems to work fine.

0 Kudos
Reply

2,119 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Dan Stahlke,

Thanks for your reply.

I don't know the reason and I'll confirm with the AE for checking.

Thanks for your information.

Have a great day,
TIC
 
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
0 Kudos
Reply