Hi Jun Zhang.
I'm using all peripherals (timers, i2c, spi, uart, pwm, caputure, rtc, dac, adc, vic,...) except USB port.
My plan is:
1) Modify hardware for replace the LPC2148 by LPC2368 in current products.
2) Move from LPC2368 to LPC1769 slowly (they are pin-compatible).
3) Move to LPC178x (lunch date oct/2013 + 15 years) after port code to LPC1769.
Do you recommend this upgrade path for the next 10 years?
NXP will extend life of LPC2368 ? Because I see that is the only part in LPC2000 remains active.
By other way, here, part LPC2368FBD100K has status "Development".
Arm7™ with 512 kB flash, 58 kB SRAM, Ethernet, USB 2.0 Device, CAN, SD/MMC, and 10-bit ADC | NXP
Thanks in advance!