What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What do I do with the RTCX1 and RTCX2 pins when not using the RTC on the LPC1768 ?

4,528件の閲覧回数
atkinsd84
Contributor I

Hi everyone, I'm struggling with how to terminate unused pins and the data sheet doesn't appear to have all the answers.  Can anyone help me with how to terminate pins 16 and 18 on the LPC1768 when not using the RTC.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,302件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi David,

I would recommend that RTCX1 be grounded since it is an input. RTCX2 is an output, so it can be left open.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,299件の閲覧回数
atkinsd84
Contributor I

Thanks

David Atkins

Land & Naval Defence Electronics Division

Leonardo MW Ltd

20A1-2 Ground Floor Southside PO Box 5

Southmead Road

Filton

Bristol

BS34 7QW

[email protected]<mailto:[email protected]>

Tel: +44 (0) 117 931 3556

Mob: +44 (0) 7793422675

HELICOPTERS / AERONAUTICS / ELECTRONICS, DEFENCE AND SECURITY SYSTEMS / SPACE

0 件の賞賛
返信