Hello,
I am flashing my code through Flash Magic over UART0, just wanted to know whether I can Flash it over other UART ?
If I understood correctly, the boot ROM is configured to receive data from UART0. How can we configure to receive data from UART3 ?
Thanks in Advance
Hi Ashok Rabadiya,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) If I understood correctly, the boot ROM is configured to receive data from UART0. How can we configure to receive data from UART3?
-- No, I'm afraid the UART3 is unavailable
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
 Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------