Updating firmware using UART for LPC1768

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating firmware using UART for LPC1768

1,399件の閲覧回数
ashokrabadiya
Contributor I

Hello,

 

I am flashing my code through Flash Magic over UART0, just wanted to know whether I can Flash it over other UART ? 

 

If I understood correctly, the boot ROM is configured to receive data from UART0. How can we configure to receive data from UART3 ?

 

Thanks in Advance

ラベル(1)
0 件の賞賛
返信
1 返信

1,302件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ashok Rabadiya,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) If I understood correctly, the boot ROM is configured to receive data from UART0. How can we configure to receive data from UART3?
-- No, I'm afraid the UART3 is unavailable

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信