USB0_VBUS current draw higher than expected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB0_VBUS current draw higher than expected

3,562件の閲覧回数
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by jsdmichaud on Wed Feb 25 13:39:56 MST 2015
Hello,

We are working on a product that can be powered by USB. The uC used is the LPC4357. The VDDIO of the LPC4357 is seperate from the USB power. It can happen that the USB power is present on the board while the VDDIO is not present (regulator shutdowned). Looking to the LPC43xx user manual and the AN11392 application note, we learned that the USBx_VBUS (USB0_VBUS in our case) pin are 5V tolerant only when VDDIO power of the LPC is present.

So we needed a way to reduce the USB voltage at the USB0_VBUS. In the AN11392 application note there's a recommended solution by using a voltage divider with a 24kohm and a 39kohm resistor. This solution doesn't work for us because the voltage measured at the USB0_VBUS pin is a lot lower than expected.

So we tried another solution by using a series resistor and a simple diode between the USB0_VBUS pin and our 3.3V power bus, which is the VDDIO voltage of the LPC. Attached is the little circuit we used toreduce the voltage at USB0_VBUS. Here are results of what we measured:


- When VUSB is at 5V and the 3.3V bus (VDDIO) is not active, voltage measured at USB0_VBUS is 1.7V. We get this result because the 3.3V is around 1V (not 0V) because of the voltage going accross the protection diode in the LPC4357 because VDDIO is not present. So 1V + Vf of the diode = 1.7V

- When VUSB is at 5V and the 3.3V bus (VDDIO) is active and we are in the bootloader of the application (no initialization of the USB interface), voltage measured at USB0_VBUS is 4V. **We were expecting (3.3V + Vf of the diode) = 4V. So this is correct at this point.

- When VUSB is at 5V and the 3.3V bus (VDDIO) is active and the initialization of the USB interface is done, voltage measured at USB0_VBUS is 2.9V. **We were expecting (3.3V + Vf of the diode) = 4V. At this point USB0_VBUS pin seems to draw too much current. (5V - 2.8V)/ 1000ohm = 2.2mA which seems a lot for this kind of pin.

This current draw could also be the cause of the problem with the voltage divider solution recommended in the AN11392 application note.

Is there any other solution ? And, is it normal that this pin is acting like that when the USB is initialized in the application code.

Thnaks a lot

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,443件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by username1039r48 on Sat Feb 13 19:51:06 MST 2016
For anyone experiencing the same issue: The 2mA current draw is most likely caused by the vbus discharge bit being set (bit OTGSC->VD, see 25.6.16 in the LPC43xx user manual). This enables an internal pulldown of about 1.2kOhm.

The usb library sets this bit by default, which is a bug i think.

If you disable the bit right after calling USB_Init(), a voltage divider should work just fine:



Quote:

USB_Init(corenum, USB_MODE_Device);
LPC_USB0->OTGSC &= ~(1<<0);



The current consumed by the Vbus pin in this case is < 50uA instead of 2mA.
0 件の賞賛
返信

3,443件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gregd on Tue Mar 03 07:45:29 MST 2015
We have found that different revisions of the LPC4350 silicon require different currents to pull UP the USB0_VBUS line to a valid logic high.  We originally used a 15K series resistor between the USB cable 5V pin and the USB0_VBUS pin on the LPC4350 and a 33.2K resistor in parallel with a 3.6 V zener diode from the USB0_VBUS pin to ground.  We had to change the series 15K to a 1K to work on older revision silicon. 
For example, it did not work with the following marked part:
LPC4359FET256
PFM906.4      10
ESD1149ZRY

Newer versions of the silicon worked ok with the 15 K series resistor:
LPC4350FET256
SC4K9         20
9SD14190C

0 件の賞賛
返信

3,443件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by boscfab on Thu Feb 26 01:09:49 MST 2015
Hi,
in the past I have had a similar problem but I have had no response.
I have found an abnormal absorption on pin VBUS0 when the MCU is turned on in BOOT mode for programming with DFU via USB0: http://www.lpcware.com/content/forum/lpc4357-problem-usb0-dfu-mode

The solution I adopted has been to use two small MOSFET as shown in the attached image.

BR

Fabio
0 件の賞賛
返信