USB in M0 on lpc43xx.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB in M0 on lpc43xx.

1,130 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mgordon@nxcsystems.com on Sat Jul 12 17:11:26 MST 2014
I'm trying to get the usbd_rom working in the M0 on an lpc4350.  I have the M0 running just fine, I am using the vcom and uart projects from the LPCOpen examples, they work fine when running in the M4, but will not work in the M0.  Are there changes to the code needed to get them to work properly in the M0?  I've linked them against the proper M0 libraries, and such.

标签 (1)
0 项奖励
回复
1 回复

1,079 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Jul 18 10:33:35 MST 2014
Hi
Have you tried the dual core usbd_msc example from LPCOpen ? It can be used as a good starting point.

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages


Thanks,
NXP Technical Support
0 项奖励
回复