USB in M0 on lpc43xx.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB in M0 on lpc43xx.

1,480件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Sat Jul 12 17:11:26 MST 2014
I'm trying to get the usbd_rom working in the M0 on an lpc4350.  I have the M0 running just fine, I am using the vcom and uart projects from the LPCOpen examples, they work fine when running in the M4, but will not work in the M0.  Are there changes to the code needed to get them to work properly in the M0?  I've linked them against the proper M0 libraries, and such.

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,429件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Jul 18 10:33:35 MST 2014
Hi
Have you tried the dual core usbd_msc example from LPCOpen ? It can be used as a good starting point.

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages


Thanks,
NXP Technical Support
0 件の賞賛
返信