USB detection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB detection

994 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pradeep Kumar on Tue May 28 06:02:02 MST 2013

We are working on fdi lpc3250 board. we are trying to verify the attached usb in OHCI mode.
On giving this command ls -l /proc/bus/usb
we are getting the following result
 ~ # ls -l /proc/bus/usb/
dr-xr-xr-x    2 root     root            0 Jan  1 00:00 001
-r--r--r--    1 root     root            0 Jan  1 00:00 devices

We are not getting the line

  -r--r--r-- 1 root root 0  Sep 19  22:30  drivers


Are we missing something.

In linux uboot also we are able to detect pen drive but it is getting reset.

Please do help us out if possible

Regards,

Pradeep                 

标签 (1)
0 项奖励
回复
0 回复数