USB detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB detection

965 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pradeep Kumar on Tue May 28 06:02:02 MST 2013

We are working on fdi lpc3250 board. we are trying to verify the attached usb in OHCI mode.
On giving this command ls -l /proc/bus/usb
we are getting the following result
 ~ # ls -l /proc/bus/usb/
dr-xr-xr-x    2 root     root            0 Jan  1 00:00 001
-r--r--r--    1 root     root            0 Jan  1 00:00 devices

We are not getting the line

  -r--r--r-- 1 root root 0  Sep 19  22:30  drivers


Are we missing something.

In linux uboot also we are able to detect pen drive but it is getting reset.

Please do help us out if possible

Regards,

Pradeep                 

Labels (1)
0 Kudos
Reply
0 Replies