USB detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB detection

964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pradeep Kumar on Tue May 28 06:02:02 MST 2013

We are working on fdi lpc3250 board. we are trying to verify the attached usb in OHCI mode.
On giving this command ls -l /proc/bus/usb
we are getting the following result
 ~ # ls -l /proc/bus/usb/
dr-xr-xr-x    2 root     root            0 Jan  1 00:00 001
-r--r--r--    1 root     root            0 Jan  1 00:00 devices

We are not getting the line

  -r--r--r-- 1 root root 0  Sep 19  22:30  drivers


Are we missing something.

In linux uboot also we are able to detect pen drive but it is getting reset.

Please do help us out if possible

Regards,

Pradeep                 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)