USB 2.0 High Speed at 1.8 V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 2.0 High Speed at 1.8 V

Jump to solution
2,182 Views
alex10
Contributor I

Are there any NXP MCUs that support USB 2.0 High Speed when operating at 1.8 V? It seems that most of them require 3.0 V to use USB HS.

0 Kudos
Reply
1 Solution
2,094 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, we don't have MCUs with this requirement. 

Regards

Sol 

View solution in original post

0 Kudos
Reply
2 Replies
2,095 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, we don't have MCUs with this requirement. 

Regards

Sol 

0 Kudos
Reply
2,094 Views
alex10
Contributor I

Hi Sol,

Thank you for the response.

-Alex

0 Kudos
Reply