UM10850 damaged.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UM10850 damaged.

13,862 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Tue Dec 16 23:27:58 MST 2014
I'd like to ask NXP not to 'copy protect' the User's Manuals and datasheets.
[list=1]
  [*]Opening the UM10850 in my Web-browser (any of my Web-browsers) crashes them immediately.
  [*]Find (search) does not work.
  [*]The TOC does not work, it's messed up completely and clicking it does not work either.
  [*]NO links work inside the document.
  [*]One can buy software, which removes the protection anyway.
  [*]The only way to find what you're looking for is to page up/page down through the document.
[/list]

All these problems are encountered when using Mac OS X 10.5.8.

[img=256x222]http://www.lpcware.com/system/files/Picture%20418.png[/img]
Labels (1)
0 Kudos
Reply
13 Replies

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Mon Dec 22 16:00:24 MST 2014

Quote:
At the risk of causing a flame war



In this case I find it better not to respond. The answer to your suggestions is already written above anyway.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Mon Dec 22 15:59:12 MST 2014
I uploaded the PDF I downloaded earlier, and the SHA256 match exactly.
-I expected that, because last time NXP removed encryption from one of their User's Manuals, that fixed the problem as well.
Last time was for the LPC1788 (I needed that UM for helping someone else, and had to use Rev2.0 instead of the newest Rev2.1).
This time I also needed to help someone else, but I do not have an old PDF, which works better, so I can't continue helping him with it.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Mon Dec 22 09:45:37 MST 2014
At the risk of causing a flame war...

If the browser crashes, that is a problem with YOUR BROWSER.

Seeing as you, with old and out of date, software are the only person reporting an issue, the problem must be at your end.

Upgrade your software.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Mon Dec 22 08:44:25 MST 2014
I have a Windows PC, but at least I can see that it is encrypted and seems to use:

Security method: password security
Encryption level: 128-bit RC4

Seems to be some kind of protection against modifying the PDF.

But have you taken into account, that perhaps download has failed (too small file, changed file, ...)?
I have just downloaded the file and took virustotal ( https://www.virustotal.com ) to calculate SHA256:
It is "f86363de8baa8b005f074ea2fe3ee72654aa1408ac44be94afb77299be1ce624".
Can you take your (already downloaded) file and calculate the same checksum? Is it equal?
0 Kudos
Reply

13,812 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Mon Dec 22 08:28:11 MST 2014
I really don't see why you must encrypt the documents.
It seems to be very random to me, whether they're encrypted or not, and it does not help anyone anyway.
Most of your PDF files are unencrypted, so they cause no problems; but when I hit one that's encrypted, the browser crashes, causing strong frustration on my side, because I do not just use a single window when I look for information on the Web (it's really causing great pain every time it happens).

So my wish this Christmas is this: I'd like NXP to start making the public PDFs unencrypted (perhaps set some preferences that makes unencrypted PDFs the default, if such preferences exists).
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Dec 22 01:26:00 MST 2014
I am sorry, but this must be a problem with your viewer. Standard Adobe tools are used to create the documents. As you can see from the attached screenshot, the data is not garbled and the PDF was created by Acrobat Distiller v10.1.9 on Windows.

[img]http://www.lpcware.com/system/files/screen-capture-1_0.png[/img]
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Sun Dec 21 22:26:13 MST 2014

Quote: nerd herd
I've verified that the LPC5410x UM in particular does not have any copy protection and that the TOC, search, etc. functions as it should on Windows 7, OSX 10.8.5, and Arch Linux.



Note: Mac OS X 10.8.5 is not the same as Mac OS X 10.5.8...

[img=256x272]http://www.lpcware.com/system/files/Picture%20419.png[/img]
Note that the inspector-window shows garbled content.

[img=256x216]http://www.lpcware.com/system/files/Picture%20420.png[/img]
Note that the file is encrypted.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Sun Dec 21 22:18:47 MST 2014
Adobe reader does not fix my browser crashes.

When I click a .PDF document, they usually cause no problems, but if I click one of NXP's PDF documents, there's a 10% chance that it will crash my browser, and thus all my windows will be trashed (including some of my browsing history, so if I'm in the middle of something, I'll have to try and remember how I got there).
The right fix is to produce PDF-files that are not damaged by incorrect data.
All the PDF files I produce (eg. author) are 100% correct and can be read by everyone.
There is some PDF generator out there somewhere, which produces incorrect data, when it's encrypting the pages.
The solution is to generate the PDFs without the "encrypt" checkbox checked. It's fairly simple and easy; and it causes the PDFs to be readable by everyone, including older systems.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri Dec 19 11:09:11 MST 2014
How about using the Adobe reader?
http://www.macupdate.com/app/mac/73/adobe-reader
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Fri Dec 19 11:00:25 MST 2014
I cannot change my software, and Apple does not want to update it.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Fri Dec 19 10:58:25 MST 2014
I've seen it with so many PDF files made by NXP, and I've sent a note to support as well.
The problem happens whenever the PDF is encrypted, it does not happen when a PDF is unencrypted.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Wed Dec 17 11:58:02 MST 2014
Hi Pacman,

I'm sorry to hear that you can't open the PDF in your browser and many of the functions do not work. I've verified that the LPC5410x UM in particular does not have any copy protection and that the TOC, search, etc. functions as it should on Windows 7, OSX 10.8.5, and Arch Linux.
0 Kudos
Reply

13,815 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Dec 17 00:05:07 MST 2014
No problems here. Nothing wrong with the PDF at all (OSX 10.9). Probably a problem with your (very old) software.
0 Kudos
Reply