UART connection for LPC55S28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART connection for LPC55S28

1,007件の閲覧回数
steve5528
Contributor I

Good day!

 

I am building a PCB with LPC55S2x and would like to know the hardware level specifics to make UART work? If for instance, FC0 UART is being used, then, is it simple as routing the two FC0 pins: RXD and TXD to a jumper from where a serial-usb bridge is used to connect to the PC? Do RX and TX lines need any resistors on their path? In EVK-LPC55S2x schematics, I see FC0_USART_RXD connecting to a 100 ohm resistor, so wanted some clarification.

 

Thanks.

0 件の賞賛
返信
1 返信

977件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @steve5528 

We highly recommend that you refer to the schematic of the LPCxpresso55s28.

https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...  

 

BR

Alice

0 件の賞賛
返信