The GPIO of LPC1125 cannot output low level, why?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The GPIO of LPC1125 cannot output low level, why?

ソリューションへジャンプ
1,733件の閲覧回数
Wei_Lang
Contributor II

The GPIO of the LPC1125 cannot output low level, why?

main();

int main (void) {
	SystemCoreClockUpdate();//LPC1125 Clock Settings. LPC1125时钟设置
	LPC_SYSCON->SYSAHBCLKCTRL |= (1UL << 6 | 1UL << 16);
	/* enable clock for GPIO */
	LPC_IOCON->PIO2_0 = 0xD0;
	LPC_IOCON->PIO2_1 = 0xD0;
	LPC_IOCON->PIO2_2 = 0xD0;
	LPC_GPIO2->DIR = 0x07;
	LPC_GPIO2->MASKED_ACCESS[0x07] = 0;
	//However, PIO2_0 is always high, and cannot output low level. The program downloads normally.
	//但是PIO2_0始终是高电平,无法输出低电平。程序下载正常。
}

 

SystemCoreClockUpdate();

void SystemCoreClockUpdate (void)               /* Get Core Clock Frequency   */
{
  uint32_t oscClk = 0;

  /* Determine clock frequency according to clock register values             */
  switch ((LPC_SYSCON->WDTOSCCTRL >> 5) & 0x0F) {
    case 0:  oscClk =       0; break;
    case 1:  oscClk =  600000; break;
    case 2:  oscClk = 1050000; break;
    case 3:  oscClk = 1400000; break;
    case 4:  oscClk = 1750000; break;
    case 5:  oscClk = 2100000; break;
    case 6:  oscClk = 2400000; break;
    case 7:  oscClk = 2700000; break;
    case 8:  oscClk = 3000000; break;
    case 9:  oscClk = 3250000; break;
    case 10: oscClk = 3500000; break;
    case 11: oscClk = 3750000; break;
    case 12: oscClk = 4000000; break;
    case 13: oscClk = 4200000; break;
    case 14: oscClk = 4400000; break;
    case 15: oscClk = 4600000; break;
  }
  oscClk /= ((LPC_SYSCON->WDTOSCCTRL & 0x1F) << 1) + 2;

  switch (LPC_SYSCON->MAINCLKSEL & 0x03) {
    case 0:                                     /* Internal RC oscillator     */
      SystemCoreClock = __IRC_OSC_CLK;
      break;
    case 1:                                     /* Input Clock to System PLL  */
      switch (LPC_SYSCON->SYSPLLCLKSEL & 0x03) {
        case 0:                                 /* Internal RC oscillator     */
          SystemCoreClock = __IRC_OSC_CLK;
          break;
        case 1:                                 /* System oscillator          */
          SystemCoreClock = __SYS_OSC_CLK;
          break;
        case 2:                                 /* Reserved                   */
        case 3:                                 /* Reserved                   */
          SystemCoreClock = 0;
          break;
      }
      break;
    case 2:                                     /* WDT Oscillator             */
      SystemCoreClock = oscClk;
      break;
    case 3:                                     /* System PLL Clock Out       */
      switch (LPC_SYSCON->SYSPLLCLKSEL & 0x03) {
        case 0:                                 /* Internal RC oscillator     */
          if (LPC_SYSCON->SYSPLLCTRL & 0x180) {
            SystemCoreClock = __IRC_OSC_CLK;
          } else {
            SystemCoreClock = __IRC_OSC_CLK * ((LPC_SYSCON->SYSPLLCTRL & 0x01F) + 1);
          }
          break;
        case 1:                                 /* System oscillator          */
          if (LPC_SYSCON->SYSPLLCTRL & 0x180) {
            SystemCoreClock = __SYS_OSC_CLK;
          } else {
            SystemCoreClock = __SYS_OSC_CLK * ((LPC_SYSCON->SYSPLLCTRL & 0x01F) + 1);
          }
          break;
        case 2:                                 /* Reserved                   */
        case 3:                                 /* Reserved                   */
          SystemCoreClock = 0;
          break;
      }
      break;
  }
  SystemCoreClock /= LPC_SYSCON->SYSAHBCLKDIV;
}

 

SYSAHBCLKCTR

SYSAHBCLKCTRL
bit	Symbol	Value	Description
6	GPIO	0		Disable clock for GPIO.
			1		Enable *

16	IOCON	0		Disable clock for I/O configuration block.
			1		Enable *

 

LPC_GPIO2->DIR

LPC_GPIO2->MASKED_ACCESS

/*------------- General Purpose Input/Output (GPIO) --------------------------*/
/** @addtogroup LPC112x_GPIO LPC112x General Purpose Input/Output 
  @{
*/
typedef struct
{
  union {
    __IO uint32_t MASKED_ACCESS[4096];  /*!< Offset: 0x0000 to 0x3FFC Port data Register for pins PIOn_0 to PIOn_11 (R/W) */
    struct {
         uint32_t RESERVED0[4095];
    __IO uint32_t DATA;                 /*!< Offset: 0x3FFC Port data Register (R/W) */
    };
  };
       uint32_t RESERVED1[4096];
  __IO uint32_t DIR;                    /*!< Offset: 0x8000 Data direction Register (R/W) */
  __IO uint32_t IS;                     /*!< Offset: 0x8004 Interrupt sense Register (R/W) */
  __IO uint32_t IBE;                    /*!< Offset: 0x8008 Interrupt both edges Register (R/W) */
  __IO uint32_t IEV;                    /*!< Offset: 0x800C Interrupt event Register  (R/W) */
  __IO uint32_t IE;                     /*!< Offset: 0x8010 Interrupt mask Register (R/W) */
  __I uint32_t RIS;                    /*!< Offset: 0x8014 Raw interrupt status Register (R/ ) */
  __I uint32_t MIS;                    /*!< Offset: 0x8018 Masked interrupt status Register (R/ ) */
  __O uint32_t IC;                     /*!< Offset: 0x801C Interrupt clear Register (/W) */
} LPC_GPIO_TypeDef;


//However, PIO2_0 is always high, and cannot output low level. The program downloads normally.
//但是PIO2_0始终是高电平,无法输出低电平。程序下载正常。

ラベル(3)
0 件の賞賛
返信
1 解決策
1,656件の閲覧回数
Wei_Lang
Contributor II

1. SWDIO/PIO1_3, add external 4.7K to 10K pull up resistor. SWD_CLK don't add external circuit.
2. RESET/PIO0_0, should add 4.7K to 10K pull up resistor, and 0.1uf Capacitor to ground.
3. P0_1, should add 4.7K to 10K pull up resistor.
4. Check the schematic diagram and select the correct PIO2_0.

Wei Lang

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,657件の閲覧回数
Wei_Lang
Contributor II

1. SWDIO/PIO1_3, add external 4.7K to 10K pull up resistor. SWD_CLK don't add external circuit.
2. RESET/PIO0_0, should add 4.7K to 10K pull up resistor, and 0.1uf Capacitor to ground.
3. P0_1, should add 4.7K to 10K pull up resistor.
4. Check the schematic diagram and select the correct PIO2_0.

Wei Lang

0 件の賞賛
返信
1,722件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Just after  a brief review, can you use the code and test the pin:

change

LPC_GPIO2->MASKED_ACCESS[0x07] = 0;

to

LPC_GPIO2->MASKED_ACCESS[4095] = 0;

Pls have a try

BR

XiangJun Rong

0 件の賞賛
返信
1,716件の閲覧回数
Wei_Lang
Contributor II

It cannot solve when I changing to : 

LPC_GPIO2->MASKED_ACCESS[4095] = 0;

There may be other problems.

0 件の賞賛
返信