Support for LPC4370

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for LPC4370

1,687件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Fri Nov 01 05:58:35 MST 2013
Hi,

I cannot find any header file, for example, LPC43xx.h, that contains definitions for both M0 processors on the LPC4370 chip.

LPC43xx.h only contains definitions for M4 and a single M0 processor. From a brief look at the code for the  LPC LabTool it looks as if only the M4 core is used?

Could somebody please show me where to find the right header file for this device.

Thanks in advance,

JohnR
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,671件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Wed Nov 06 18:52:19 MST 2013
Hi drs,

Thank you - I will take a look at it.

John.
0 件の賞賛
返信

1,668件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Wed Nov 06 12:22:55 MST 2013
Hi John,

We have not created header files with a formal definition of the third core yet. This is coming soon. However we do have a triple core example which is attached here. It is based on the Keil tool and uses the header files from the tool's example repository.

Hope this helps.
0 件の賞賛
返信