Support for LPC4370

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for LPC4370

1,679 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Fri Nov 01 05:58:35 MST 2013
Hi,

I cannot find any header file, for example, LPC43xx.h, that contains definitions for both M0 processors on the LPC4370 chip.

LPC43xx.h only contains definitions for M4 and a single M0 processor. From a brief look at the code for the  LPC LabTool it looks as if only the M4 core is used?

Could somebody please show me where to find the right header file for this device.

Thanks in advance,

JohnR
Labels (1)
0 Kudos
Reply
2 Replies

1,663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JohnR on Wed Nov 06 18:52:19 MST 2013
Hi drs,

Thank you - I will take a look at it.

John.
0 Kudos
Reply

1,660 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Wed Nov 06 12:22:55 MST 2013
Hi John,

We have not created header files with a formal definition of the third core yet. This is coming soon. However we do have a triple core example which is attached here. It is based on the Keil tool and uses the header files from the tool's example repository.

Hope this helps.
0 Kudos
Reply