State Configurable Timer on LPC1830 to measure input signal H,V?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

State Configurable Timer on LPC1830 to measure input signal H,V?

766 Views
kensu
Contributor V

Dear Sirs,

I have a purpose to measure input signal H,V total clock (ex:  input signal with external H,V sync clock input).

Is it possible to use SCT counter to measure the H,V clock?

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

628 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

1) Is it possible to use SCT counter to measure the H,V clock?
Yes, of course.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply