I have a lidar sensor and its output is PWM . I want to give that pwm output as a input to lpc 1758 and want to read the output of that . Currently i am using lpc 1758. I don't know about which and how I use peripheral. i want to use 6 pwm inputs at a tim

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have a lidar sensor and its output is PWM . I want to give that pwm output as a input to lpc 1758 and want to read the output of that . Currently i am using lpc 1758. I don't know about which and how I use peripheral. i want to use 6 pwm inputs at a tim

1,098 Views
ashrinshaikh
Contributor I

II have a lidar sensor and its output is PWM . I want to give that pwm output as a input to lpc 1758 and want to read the output of that . Currently i am using lpc 1758. I don't know about which and how I use peripheral. i want to use 6 pwm inputs at a time. please give me any suggestion or any sample code?

Labels (1)
0 Kudos
Reply
1 Reply

954 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ashrin Shaikh,

I've already answered the thread: programming of lpc 1758 pwm ?
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply