State Configurable Timer on LPC1830 to measure input signal H,V?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

State Configurable Timer on LPC1830 to measure input signal H,V?

1,126 次查看
kensu
Contributor V

Dear Sirs,

I have a purpose to measure input signal H,V total clock (ex:  input signal with external H,V sync clock input).

Is it possible to use SCT counter to measure the H,V clock?

Thanks

标签 (1)
0 项奖励
回复
1 回复

988 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Su,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

1) Is it possible to use SCT counter to measure the H,V clock?
Yes, of course.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复