Slave I2C1 Test with master I2C0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slave I2C1 Test with master I2C0

1,444 Views
kensu
Contributor V

Hi

I am implement the I2C slave function.

I am using MCB1857 EVA board, I want to confirm if I can set I2C0 to master and set I2C1 to slave mode,

and connect each SCL and SDA to transmit data(i2c0 sends to i2c1)?

Is it work?

Thanks

Ken

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,324 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Ken Su,

    Of course you can!

    I2C0 and I2C1 are the independent module.

   You can use any one as master, and another one as slave.

   Just do it.

Wish it helps you!

   


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply