Slave I2C1 Test with master I2C0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Slave I2C1 Test with master I2C0

937 次查看
kensu
Contributor V

Hi

I am implement the I2C slave function.

I am using MCB1857 EVA board, I want to confirm if I can set I2C0 to master and set I2C1 to slave mode,

and connect each SCL and SDA to transmit data(i2c0 sends to i2c1)?

Is it work?

Thanks

Ken

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

817 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Ken Su,

    Of course you can!

    I2C0 and I2C1 are the independent module.

   You can use any one as master, and another one as slave.

   Just do it.

Wish it helps you!

   


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复