Slave I2C No interrupt when Data Received

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Slave I2C No interrupt when Data Received

ソリューションへジャンプ
3,475件の閲覧回数
kensu
Contributor V

Hi,

I am using LPC1830 slave i2c, there is an issue.

For slave i2c, it use interrupt to receive data. I check the i2c waveform, the LPC1830 HW is correct, all bytes from master are received because each byte have ACK from LPC1830.

But in SW, the interrupt only happen when all transaction is complete, it means the interrupt will only 1 times no matter how many bytes send.

The correct behavior should be each byte will trigger an interrupt and the i2c slave RX buffer receive these bytes.

I don't know why only all transaction is complete, and it will trigger one interrupt.

(I had evaluate the same source code on LPC1857, it's work. But for LPC1830, it's fail)

Please give me some comment.

Thanks

Ken

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,044件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Ken,

   Thank you very much for your updated information and the root problem.

   If your question is solved, please mark the correct answer to close this post, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,044件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ken Su,

     The SI is the I2C interrupt Flag, this bit is set when the I2C state changes.

pastedImage_1.png

   So, you can check your I2C state, whether the state is changed?

Besides, I find in the errata, there has some descriptions about the I2C, you can do the work-around about it.

pastedImage_2.png

Wish it helps you!

If you still have question about it, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,044件の閲覧回数
kensu
Contributor V

Hi

Thanks you for reply,

I had find my software bug for this issue.

Thank you

Ken

0 件の賞賛
返信
3,045件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Ken,

   Thank you very much for your updated information and the root problem.

   If your question is solved, please mark the correct answer to close this post, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信