Setting up pyOCD with LPC-Link2 Debugger and LPC54102J512 MCU.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting up pyOCD with LPC-Link2 Debugger and LPC54102J512 MCU.

1,975件の閲覧回数
tleggas
Contributor I

I am using pyOCD v0.35.1 and Python v3.10.6 to try flashing an LPC54102. I have installed the available USB drivers, installed CMSIS-DAP firmware to the Link2 using LPCScrypt, and verified that the debugger probe is functioning by flashing with FlashMagic. I have also installed the LPC54102 CMSIS pack to pyocd.

When I run pyocd list, all I get is "No available debug probes are connected."

Any thoughts on what I may be missing?

Thanks.

0 件の賞賛
返信
1 返信

1,958件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tleggas 

How about refer to the below thread:

https://community.nxp.com/t5/LPC-Microcontrollers/How-to-flash-a-LPC1114-with-pyocd-or-openocd-using...  

And I just wonder why do not use IDE to debug? 

 

BR

Alice

0 件の賞賛
返信