Setting up pyOCD with LPC-Link2 Debugger and LPC54102J512 MCU.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting up pyOCD with LPC-Link2 Debugger and LPC54102J512 MCU.

1,985 次查看
tleggas
Contributor I

I am using pyOCD v0.35.1 and Python v3.10.6 to try flashing an LPC54102. I have installed the available USB drivers, installed CMSIS-DAP firmware to the Link2 using LPCScrypt, and verified that the debugger probe is functioning by flashing with FlashMagic. I have also installed the LPC54102 CMSIS pack to pyocd.

When I run pyocd list, all I get is "No available debug probes are connected."

Any thoughts on what I may be missing?

Thanks.

0 项奖励
回复
1 回复

1,968 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tleggas 

How about refer to the below thread:

https://community.nxp.com/t5/LPC-Microcontrollers/How-to-flash-a-LPC1114-with-pyocd-or-openocd-using...  

And I just wonder why do not use IDE to debug? 

 

BR

Alice

0 项奖励
回复