SYSCON_PDRUNCFG_PD_IRC_OSC vs SYSCON_PDRUNCFG_PD_IRC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SYSCON_PDRUNCFG_PD_IRC_OSC vs SYSCON_PDRUNCFG_PD_IRC

ソリューションへジャンプ
2,495件の閲覧回数
simonwyss
Contributor III

What is the difference between these two Power Switches? 

LPCopen file: syscon_5410x.h

SYSCON_PDRUNCFG_PD_IRC_OSC

SYSCON_PDRUNCFG_PD_IRC

pastedImage_5.png

ラベル(1)
1 解決策
2,377件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Simon Wyss,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Keep mind: To enable the IRC oscillator, these two bits should work together, they're inseparable.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,378件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Simon Wyss,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Keep mind: To enable the IRC oscillator, these two bits should work together, they're inseparable.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,377件の閲覧回数
simonwyss
Contributor III

Hi jeremyzhou 
Thank you for your reply!

0 件の賞賛
返信