SYSCON_PDRUNCFG_PD_IRC_OSC vs SYSCON_PDRUNCFG_PD_IRC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SYSCON_PDRUNCFG_PD_IRC_OSC vs SYSCON_PDRUNCFG_PD_IRC

Jump to solution
2,510 Views
simonwyss
Contributor III

What is the difference between these two Power Switches? 

LPCopen file: syscon_5410x.h

SYSCON_PDRUNCFG_PD_IRC_OSC

SYSCON_PDRUNCFG_PD_IRC

pastedImage_5.png

Labels (1)
1 Solution
2,392 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Simon Wyss,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Keep mind: To enable the IRC oscillator, these two bits should work together, they're inseparable.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,393 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Simon Wyss,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Keep mind: To enable the IRC oscillator, these two bits should work together, they're inseparable.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,392 Views
simonwyss
Contributor III

Hi jeremyzhou 
Thank you for your reply!

0 Kudos
Reply