SJA1105Q-EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105Q-EVB

Jump to solution
1,453 Views
哈哈哈哈哈
Contributor I

_0-1768356546887.png

Hello, in the SJA1105Q-EVB evaluation board, the 3.3V enable pin VREG_EN can be controlled as shown in the figure. What is the process and principle between the control by the LPC1788FET208 main chip pin MCU_VREG_INH and the control by the J9 jumper?

0 Kudos
Reply
1 Solution
1,393 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @哈哈哈哈哈 

 

On the SJA1105Q‑EVB, the 3.3 V power enable signal (VREG_EN) is typically controlled through two paths:

  1. A control signal from the MCU (LPC1788), MCU_VREG_INH.
  2. A hardware override via the J9 jumper, which can directly force VREG_EN on or off.
    When J9 is used, it bypasses the MCU control path.

 

Thank you.

BR

Alice

View solution in original post

0 Kudos
Reply
2 Replies
1,393 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @哈哈哈哈哈 

 

On the SJA1105Q‑EVB, the 3.3 V power enable signal (VREG_EN) is typically controlled through two paths:

  1. A control signal from the MCU (LPC1788), MCU_VREG_INH.
  2. A hardware override via the J9 jumper, which can directly force VREG_EN on or off.
    When J9 is used, it bypasses the MCU control path.

 

Thank you.

BR

Alice

0 Kudos
Reply
1,232 Views
哈哈哈哈哈
Contributor I
If J9 pins 1 and 2 are shorted, control comes from the PHY, meaning the MAC will also lose power. How can it be awakened then?
0 Kudos
Reply