S12ZVC or LPC11C24 Mbed Support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVC or LPC11C24 Mbed Support?

1,626件の閲覧回数
joamei
Contributor I

Are S12ZVC or LPC11C24 Boards supported by Mbed? I am looking for an beginner friendly Solution for Students and Interns to work with boards that have a CAN Transceiver on board. The Arduino is very limited for stuff like this.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,498件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Christian,

Non of the MCU that you say has support for Mbed, a good option for this would be use the FRDM K64F and use an external transiver as the TJA1057, this one has support for Mbed.

For the Kinetis Family a board that has a CAN Transiver integrated is the FRDM - KEAZ128, the MCUXpress IDE has some tools that helps in the configuration of the board and its easy set up and the SDK has many examples that you can follow, including some CAN examples.

Also the S12ZVC include many examples that could help in the developing process.

Best Regards,

Alexis

0 件の賞賛
返信