Run-Time Self-Programming in LPC4370 SPIFI MODE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Run-Time Self-Programming in LPC4370 SPIFI MODE

1,280 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by park957 on Tue Apr 29 06:55:22 MST 2014


Dear,


sorry... I am not good at English.


I use that to LPC4370 SPIFI boot mode.

I want to be stored in Flash (by SPIFI).

Can I save the memory during the operation?

If possible, let me know how.


Thank you for your time.




LPC4370 + SPIFI(325FL032) + KEIL + ULINK2

标签 (1)
0 项奖励
回复
2 回复数

1,224 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by park957 on Wed May 07 00:09:40 MST 2014

Hi, bavarian

Thank you for the reply. :bigsmile:
0 项奖励
回复

1,224 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue May 06 07:44:03 MST 2014
When you do erase/program on the SPIFI you can't execute at the same time from this memory.
You need to execute from internal SRAM (or another memory) at this time.

An example can be found here: 

http://www.lpcware.com/system/files/lpcopen_2_09_keil_iar_hitex_eva_4350_1.zip

in the folder

.\lpcopen_2_09_keil_iar_hitex_eva_4350_1\applications\lpc18xx_43xx\keil_uvision_projects\hitex_eva_4350\misc\spifi_prog

Regards,
NXP Support Team
0 项奖励
回复