Run-Time Self-Programming in LPC4370 SPIFI MODE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run-Time Self-Programming in LPC4370 SPIFI MODE

1,309件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by park957 on Tue Apr 29 06:55:22 MST 2014


Dear,


sorry... I am not good at English.


I use that to LPC4370 SPIFI boot mode.

I want to be stored in Flash (by SPIFI).

Can I save the memory during the operation?

If possible, let me know how.


Thank you for your time.




LPC4370 + SPIFI(325FL032) + KEIL + ULINK2

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,253件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by park957 on Wed May 07 00:09:40 MST 2014

Hi, bavarian

Thank you for the reply. :bigsmile:
0 件の賞賛
返信

1,253件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bavarian on Tue May 06 07:44:03 MST 2014
When you do erase/program on the SPIFI you can't execute at the same time from this memory.
You need to execute from internal SRAM (or another memory) at this time.

An example can be found here: 

http://www.lpcware.com/system/files/lpcopen_2_09_keil_iar_hitex_eva_4350_1.zip

in the folder

.\lpcopen_2_09_keil_iar_hitex_eva_4350_1\applications\lpc18xx_43xx\keil_uvision_projects\hitex_eva_4350\misc\spifi_prog

Regards,
NXP Support Team
0 件の賞賛
返信