Run Code from RAM in LPC55XX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Run Code from RAM in LPC55XX

1,485 Views
pejo
Contributor III

Hello everyone,

due to the need to be able to keep using interruptions (like non blocking CAN communication) while we write in the flash block, I understand that the right solution is to run certain code from RAM.

As I understand I need to copy to ram the interruptions table, the interruption function with ALL the dependencies, functions and code used in the interruption function.

 

Can you confirm this? Do you have an example of this function?

 

Thank you!

Labels (1)
0 Kudos
Reply
3 Replies

1,458 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @pejo 

Here are some references for your convenience:

  1. MCUXpresso IDE User Guide → Section 20.13.5: Placing specific functions into RAM blocks Alice_Yang_0-1770103501156.png

     

  2.  Community Article:
    https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC-How-to-place-data-function-file-in-s... 

Please make sure to place the vector table and related ISR functions in RAM.

 

BR

Alice

0 Kudos
Reply

1,444 Views
pejo
Contributor III
Hello Alice,

thank you very much for your answer but my question is not how to do this (run a function from RAM) but which functions to place in RAM in the mentioned scenario. 

We need to grant the execution of the interruption callbacks during flash write operation.

In order to do this, which functions should be executed from RAM? Only the interruption vector and the Interruption function which we want to keep using during flash write or every dependency of the interruption function?
0 Kudos
Reply

1,408 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @pejo 

This is case‑by‑case. Any code that may be executed during a Flash write operation must run from RAM. This mainly includes the vector table, the interrupt callback functions, the drivers that will be invoked, and any other components your application may require. It depends on your specific application.
 
Thank you.
 
BR
Alice
0 Kudos
Reply